MODBUS.WATCHDOG
Description
MODBUS
ModBus is a serial communications protocol and is now the most commonly available means of connecting industrial electronic devices.
ModBus is often used to connect a supervisory computer with a remote terminal unit in supervisory control and data acquisition (SCADA) systems.
Versions of the ModBus protocol exist for serial port and Ethernet (it is widely used with TCP/IP over Ethernet).WATCHDOG is the watchdog timeout in seconds.
The Modbus
ModBus is a serial communications protocol and is now the most commonly available means of connecting industrial electronic devices.
ModBus is often used to connect a supervisory computer with a remote terminal unit in supervisory control and data acquisition (SCADA) systems.
Versions of the ModBus protocol exist for serial port and Ethernet (it is widely used with TCP/IP over Ethernet) watchdog fault, F7100, is generated if the drive does not receive any Modbus messages within a time window set by MODBUS.WATCHDOG. Zero disables the watchdog.
Context
For more information, see .
Versions
| Action | Version | Notes |
|---|---|---|
|
Implemented |
02-05-00-000 |
General Information
|
Type |
Read Write Parameter |
|
Units |
Seconds |
|
Range |
0 to 60 |
|
Default Value |
5 |
|
Data Type |
Integer |
|
See Also |
Fault F7100 |
|
Stored in Non-Volatile Memory |
Yes |